AXIS#.IL.DIFOLD

Description

AXIS#.IL.DIFOLD is the output of the drive foldback algorithm. It is an artificial current which is always above the drive continuous current, AXIS#.ICONT . When AXIS#.IL.DIFOLD is lower than AXIS#.IPEAK, it becomes the active current limit.

AXIS#.IL.DIFOLD decreases when the actual current is higher than drive continuous current and increases (up to a certain level) when the actual current is lower than drive continuous current.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Arms

Range

0 to 2,147,483.647 Arms

Default Value

N/A

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.DIFOLD

500ah

07h

Signed32

-

1000:1

Read only

No

AXIS2.IL.DIFOLD

510ah

07h

Signed32

-

1000:1

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.DIFOLD

5820

16BC

Signed32

Read Only

-

AXIS2.IL.DIFOLD

71356

116B

Signed32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.DIFOLD

5820

Float

Read Only

-